AXIS#.MOTOR.TEMP

Description

This parameter returns the motor temperature, which is represented as the resistance of the motor's PTC or NTC.

Context

For more information see Motor and Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Range

0 to 232
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
AXIS1.MOTOR.TEMP

500bh

02h

Unsigned32

-

-

Read only

Yes

AXIS2.MOTOR.TEMP

510bh

02h

Unsigned32

-

-

Read only

Yes

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.MOTOR.TEMP

6217

1849

Unsigned32

Read Only

-

AXIS2.MOTOR.TEMP

71753

1184

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.TEMP

6217

Unsigned32

Read Only

-